Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-ISC005V1 evaluation board - not getting 15V from PDO2

I bought STEVAL-ISC005V1 evaluation board from digikey, used DA45C-J3WEU  usb c type from artesyn embedded technologies.(Capable for providing 15V/3A)When i connected adapter, i got 19V from VSINK and PDO3, but i didn't get 15V from PDO2, led is not ...

MP M by Associate II
  • 1054 Views
  • 1 replies
  • 0 kudos

LED6000 use DIM as enable

Hi all,The LED6000 has a seperate EN and DIM line. I would like to use the dimming feature and also be able to disable the device. It seems I could use DIM only, and tie EN to VCC. Then, if I hold DIM low, the device should be disabled. As I use mult...

PM8805 PoE Controller Grounding

Hi,Looking at the PM8805 PoE Controller datasheet fig 7 and also AN5207 page 30 there is a 3M3 resistor from power ground to chassis ground. What it purpose, is this some form of bleed resistor to stop voltage build up? My main question though is why...

JKing.3 by Associate II
  • 881 Views
  • 0 replies
  • 0 kudos

Reference design L6562AT?

Hello,I am looking for a reference design for a PFC with an input range: 300V - 400V RMS.The output power should be 180W. Thanks.

0690X00000BwokJQAR.bmp
CCarl by Associate II
  • 680 Views
  • 0 replies
  • 0 kudos