User Activity

Hi dear,I designed a step motor driver board with L6470h and tested it. There are some problems with the board.I set the run current, hold current, ACC, ACC current, DEC, DEC current at the fixed value, and then changed the MAX speed, then the actual...
Hi,I designed a board with ​L6470h and tested it. I am confused with the Overcurrent protection function. It is shown that the capability of L6470h is 7.0 A peak current (3.0 A r.m.s.), but the MAX overcurrent threshold can be set to 6A in register...