Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STSR2P similar controller

i need controller similiar for STSR2P (secondary side synchronous rectification controller for forward topology). STSR2P has obsolete status so I need a new.

L6599 LLC resonant converter start up issue

Apply 15V at Vcc pinApply 50V at top of potential divider formed by 6M6 and 180k ohm at LINE pin in order to get LINE pin voltage >1.23VHowever, High side LLC mosfet (connected to HVG pin, on resistance: 47ohm, off resistance 10ohm) GS...

LChun.1 by Associate
  • 1116 Views
  • 0 replies
  • 0 kudos

Feed error on the STEVAL-CTM009V1 board

The supply of the STEVAL-CTM009V1 board is shown to be up to 48 V. However, the A7986ATR writes that the A6902D13TR buck converter has a maximum supply of 38V.How does this board work at 48V?Or is the feeding range of the board written wrong?

mckmk by Associate II
  • 523 Views
  • 0 replies
  • 0 kudos

How to turn off and on wireless charging using host through uart interface for stwbc-ep digital wireless charging controller ?

We are interfaced stwbc-ep with host microcontroller using uart. we want the feature to turn off charging,turn on charging based on some events. We have gone through the user manual of firmware given by st. but didn't found any register to turn off o...

Mgaon.1 by Associate
  • 680 Views
  • 0 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.