Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
BackgroundI'm using STP08DP05 to control the current (20mA) through some LEDs in my design. I'm using these for illumination purposes while I take an image. I'm finding some variation in the brightness of my image, and I think it might to do with sli...
I am trying to figure out if I can have a MPPT charge controller in parallel with a DC-DC converter (sharing a solar array). I realize the MPPT charge controller is a DC-DC converter and I am also aware that two MPPTs in parallel will cause a possibl...
Hi, We are using LD1117S50 linear regulator for conversion of 9V DC to 5V DC. The datasheet typical application diagram in page 24 suggests to use 10uF electrolytic capacitor. Please let me know whether we can use a 10uF ceramic capacitor at output. ...
The supply of the STEVAL-CTM009V1 board is shown to be up to 48 V. However, the A7986ATR writes that the A6902D13TR buck converter has a maximum supply of 38V.How does this board work at 48V?Or is the feeding range of the board written wrong?
Can this item withstand 227C work through Wave soldering / soldering production ?or any document support? thanks.
The internal resistance of "2STBN15D100" is described in the datasheet as shown below.By the way, if you actually measure the resistance between Base(1) and Emitter(3), it will measure around 12K ohm.I think that the data sheet will measure around 8K...
sample circuit need