Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VNQ7140AJ Max Working Voltage

Greeting,We are using VNQ7140AJ for high side switching power rails.Power source 28V with +%5 and -%5 tolerances. So source will be 29.4V to 26.6VIn data sheet we sow this IC's absolute maximum rating is 28V. But in page 7 data sheet says DC supply v...

EArsl.11 by Associate
  • 535 Views
  • 0 replies
  • 0 kudos

Over current/over temp on STEVAL-ISB68WA with little load

I've got the STEVAL-ISB045V1 and STEVAL-ISB68WA evaluation kits. After programming the transmitter to use the correct ping, min and max frequency parameters, I attempted to "connect" the receiver to the transmitter with a 1/4W load. When I do this,...

JDupr.2 by Associate
  • 627 Views
  • 0 replies
  • 0 kudos

LED5000 floating boost ringing issue

Hi team,i working on floating boost converter by using LED5000 IC.specifications are-Vin- 12VVout- 36V, 100mAschematic and components as per E design suite.instead of 120uH i used 47uH just for functional test.at Vin 12V my vout is 20V and LED starts...

Tanvir by Associate
  • 868 Views
  • 0 replies
  • 0 kudos

Resolved! PowerSTEP01 SW voltage level questions

Hello, I am using the powerSTEP01 chip with VDD = 3.3V and VREG = 3.3V. I would like to know if I can directly drive the "SW" (switch) input pin with a 5 Volt logic level signal. Will the pin be damaged if I drive it with a 5 Volt active level? P...

MGuru.1 by Associate II
  • 1816 Views
  • 5 replies
  • 0 kudos

Starting up a STBB1 under full load, breaks the device

I tried out the STBB1 with the evalboard to drive a load of 500mA.My trials were successfull. I did them by switching on my power supply with 5V and afterwards I was switching the 500mA Load on and off at the output. -> everything cool.Now I have my ...