Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

B-G431B-ESC1 Quadrature Encoder Generation Error

I'm getting an error "Final current ramp value is higher than motor nominal current" when I enable the quadrature encoder option in speed sensing (either as the primary or auxiliary sensor). As per another thread and the schematic, I have reconfigure...

0693W000005Bt2JQAS.png
MWild.3 by Associate II
  • 801 Views
  • 0 replies
  • 1 kudos

B-G431B-ESC1 CAN Control

I understand from the user guide and previous threads (from last year) that there is supposed to be CAN support, specifically for UAVCAN, on the B-G431B-ESC1 development kit. I wasn't able to find any examples supporting UAVCAN or even enabling the C...

MWild.3 by Associate II
  • 786 Views
  • 0 replies
  • 1 kudos

Resolved! I am having trouble getting two of the EVALMasterGAN1 evaluation boards to properly work in a full bridge configuration. Can someone help with any suggestions to fix the problem I am having?

So far, the boards are working correctly up until the Bus voltage reaches around 130Vin. Then, when monitoring the gate signals on the board at the GH and GL pin on the MasterGAN, the high side of one of the boards seems to not switch correctly anymo...

PHenr.1 by Associate II
  • 2113 Views
  • 5 replies
  • 0 kudos

Hi Dears, l have a point about VIPER06X Application Circuits,

In widely use of VIPER06X, is used to only Half-Bridge Rectifier Circuit as shown in figure, but if we need to apply it on Full-Rectifier(Bridge) Rectifier Circuit, then what should we consider?Because if we implement the grid Voltage, then can be da...

0693W000005BbHpQAK.png
MGULE.1 by Associate
  • 958 Views
  • 1 replies
  • 0 kudos

STC3115 -Current value and SOS seems updating wrongly.

Hi all,Am using STC3115 for my application and utilizing the online driver provided for stc3115 where I used only default values expect the BATT_CAPACITY in stc3115_Battery.h ,which changed that to 1100 mAh as per my battery (3.7 ,110mah).Issue is ...

dsamu.1 by Associate
  • 749 Views
  • 0 replies
  • 0 kudos

Recommendations for a synchronous linear motor or PMLSM

I'm looking to build a small linear motor, that could move or just accelerate an incoming load with permanent magnets attached along a path, like a touchless conveyor belt. https://en.wikipedia.org/wiki/Linear_motorIt might have as few as 3 or as man...

HVLED001A - issue with start up

Hi, I built my QR flyback supply for master diploma in study but I have issue with startup. When I'm starting from low voltage the transformer get strange noises to circle about 160V but I'don't have power on output, on 230V transformer is very silen...

DKlew.1 by Associate
  • 719 Views
  • 0 replies
  • 0 kudos

FOC Model in Simulink WITHOUT Simscape

Has anyone developed an FOC motor control model in MATLAB Simulink WITHOUT using SIMSCAPE? I find SIMSCAPE too confining to model the 3-phase brushless motor and interfacing signals to non-Simscape blocks.My challenge doing this is to implement SVPWM...

0693W000005BPH5QAO.jpg
BTrem.1 by Senior II
  • 1208 Views
  • 0 replies
  • 0 kudos