cancel
Showing results for 
Search instead for 
Did you mean: 

Questions about transformer design of VIPER265KDTR

朱啊啊.1
Associate

Input: Single-phase AC70-500V

Output: DC24V5W

Output diode voltage drop: 1.25V

1�?My design idea is this, design the transformer to work in CCM mode (current ripple coefficient 0.85) at the lowest input voltage and full load, and enter DCM mode after the voltage rises. The following are the transformer parameters I designed. Is it reasonable?

Estimated efficiency:75%

Core:PC40 EE19 AE:23mm²

Dmax:0.512

Number of primary turns:160

Number of secondary turns:45

VCC winding:33

Primary inductance:3.13mH

Primary wire diameter:0.2mm

VCC wire diameter:0.2mm

secondary wire diameter:0.36mm

​Sandwich wrap

2�?In addition, it is generally said that the maximum duty cycle of the flyback cannot exceed 50%, because subharmonic oscillation is prone to occur, may I ask if the duty cycle of VIPER26K can exceed 50% when designing the transformer, is there internal slope compensation?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0