Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Hi, In the evaluation board of SPV1050 (STEVAL-ISV020V1), it is mentionned that the maximum voltage from the PV cell (VMP) is to be equal 9V, but there is no indication about the absolute values that I can be supported without damaging the board. I'm...
HelloI am using in my project both brush and brushless motor. My circuit works from 1 cell lion and have dc-dc step up to 6v for my motors.My sensorless brushless motor part number is : https://www.maxongroup.com/maxon/view/configurator/BOM:ECXZ08M1V...
I am working on BMS type of system that will recondition, balance, and maintain NiMH HEV batteries. I'm considering to use L9963 IC and its accompanying evaluation board EVAL-L9963 for my prototype. My system consists of nickel-metal hydride battery ...
This data is not found on the product data sheet and it is needed for the ETL certification of one of our products (containing the L78L).A quick answer would be appreciated.ThanksMassimo
Hello, this message is addressed to ST employees, if you could please send me additional information not present in the datasheet.I'm using the EFL700A39 rechargeable solid state lithium thin film battery. I'm trying to figure out the state-of-charge...
Hi, I don't know if other people have had this problem.Actually, in the datasheet of the STEVAL-ISV020V1 is mentionned that:R1 = 10 MohmR2= 1 MohmR3 = 5.6 MohmR4 = 6.2 MohmR5 = 500 KohmR6 = 2.7 MohmHowever, when I received my evaluation board, I meas...
How can i create Custom motor details to use in Motor Control Work Bench. I am using EVSPIN32F0601S3. Any suggestions??/
Hello, Can you provide me the details whether the STEF05P electronic fuse is UL certified or not?I need to use the component in a device where the safety related components should be UL certified.Awaiting response.Best Regards,Sushant Rajbhar
Hi,I am trying to use a STEVAL_PCC009V2 board connected to a EVAL6474H board to drive a stepper motor.When I run the SPIN eval software I get a notice that the firmware is not the latest and I need to update it. I just ordered the board, but it shows...