Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Marking Information LD1117S50CTR

we have purchase this item LD1117S50CTR recently, Can i get the marking information, our QA department is asking us provide information to process production, thanks.

VICTOR1 by Associate II
  • 1387 Views
  • 1 replies
  • 0 kudos

STCH03 does not seem to detect an over voltage state

Hi,I'm testing a simple flyback converter using the STCH03L. All seems as expected, however I can not seem to get the IC to detect an overvoltage condition. To conduct the test I am simply shorting out the optocoupler. When I look at the ZCD pin the ...

0693W000006EZM4QAO.png 0693W000006EZLzQAO.png 0693W000006EZLuQAO.png

Resolved! Discharging a thin film battery - EFL700A39

Hello,I'm trying to discharge the solid state thin film lithium battery EFL700A39, with a discharge current of 0.7 mA, in the aim of reaching a state of charge of approximately 20%. Actually, the problem is the significant difference of voltages whe...

GAbi .1 by Associate II
  • 1927 Views
  • 4 replies
  • 0 kudos

SPV1050 boost start-up at Vstore=0 with low-impedance source

The datasheet (https://www.st.com/resource/en/datasheet/spv1050.pdf) mentions that the STORE voltage during initial start is charged through a charge pump, when in boost configuration.However, when I set my load to 0 V and input to 2 V, it sure seems...

Jostikas by Associate II
  • 825 Views
  • 0 replies
  • 0 kudos

SPV1050 current limiting relationship to Veoc

I have an SPV1050 configured as follows:R4 = 6.2MR5 = 1MR6 = 3.9MVeoc = 3.5VVuvp = 2.78VThe device is configured for boost mode with MPPT set to 75% and Vin = 2V. The device works as expected, except that it will only draw the full specified 70mA cu...

BLamb by Associate
  • 885 Views
  • 1 replies
  • 1 kudos

Resolved! L6984 produce wrong voltage

Hello everybody,I need a power conversion DC-DC 24V to 3.3V. So I went to eDesign suite who recommendend me the following architecture:I reproduced it in my design: I produced the board, and when I apply 24V on the input, I obtain only 0.9/1V on the ...

0693W000005CwakQAC.jpg 0693W000005Cwb9QAC.jpg
SSchm.5 by Associate III
  • 2542 Views
  • 4 replies
  • 1 kudos