Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VNH5019A-E circuit diagram configuration

Hello, I am designing a circuit using VNH5019A-E motor driver.Is there a problem if the capacitor is installed on the motor output pins OUTA and B? The value is about 10uF. For example, the charging and discharging of the capacitor leads to situation...

Oido by Associate II
  • 774 Views
  • 1 replies
  • 0 kudos

Resolved! L9961 Balancing problem.

Dear, please advice me.Balancing not working. Used Steval board with J13, J14 and all J5 open (disconnected) . HS mode.3 cells connected (C5-C4-C3) and (C2-C1-C0-GND) Used test script: WRITE60AD8N=10, Cell OV = 4.21632VWRITE70A33N=10, Cell UV = 0,995...

Pavel61 by Associate
  • 738 Views
  • 1 replies
  • 0 kudos

Modifying STEVAL-ESC001V1 for 80A Peak Current

Hi Sir,Would it be feasible to achieve an 80A peak current on this board simply by modifying the OCP circuit hardware and the corresponding firmware settings in X-CUBE-MCSDK? Or will thermal constraints and the PCB design itself (e.g., trace width, l...

TIENHUA by Associate III
  • 544 Views
  • 0 replies
  • 0 kudos

Resolved! stpm32: Is GND shared between AC and DC?

Hello everyone, I am learning about STPM32 design and I am wondering about the power source for the IC to operate. Mass (GND) is shared between AC and DC? This seems unreasonable. Hope everyone shares. knowledge.

NguyenAnhHieu__0-1758387514699.png

Resolved! L7808 Regulator 19v 20ampere Power Supply

I was design 19 volt regulated power supply, but I don't know the exact value for the transistors, and I noticed at the voltsim output didn't reach the maximum 19 volt output, can anyone help me for the solution for my design, regards.@all  

fotor_1758444679265.jpg

Speed Control problem with L6235 DIP

Posted on October 25, 2016 at 20:05Hi All,I want to make a BLDC motor driver board using L6235N DIP.I wired all the components on the breadboard as per schematic diagram and component list is given in ST Application Note AN1625 page no. 35-37.I am u...

vkyadav by Associate
  • 1536 Views
  • 2 replies
  • 0 kudos

Resolved! FDA803S/FDA903S

I need more information about FDA803S on website there aren't document explaining I2C registers and details about connection of configurable pins (eq ENABLE1 an 2) There is a firmware example for use this device connected to a stm32 microcontroller?

BTA24-800CW can't switch off 60 W resistive lump

i am using MOC3063 as an optocoupler and BTA24-800CW as a triac .with 220 V ac and it worked fine (switch on and off) with the 10W,5W,3W resistive loads but when using 60 W incandescent lump it only turn on but not off   i am using this basic circui...

momensalah_0-1753671467464.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.