Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STWLC68 Debug/Program

Hi,I see that STWLC68 has a 32-bit 64 MHz ARM Cortex microcontroller core. How can I program or debug this device using STM32CubeIDE. I'm not able to create a project with this device.gaston

Gaston by Senior
  • 1101 Views
  • 2 replies
  • 0 kudos

SPV1050 - VMPP range in datasheet?

Hi,In the SPV1050 datasheet, in the Electrical characteristics section, the VMPP voltage range is defined as 0.075V to VUVP - 0.1V. I do not understand why VMPP is limited by VUVP. In buck-boost configuration, certainly the input source's maximum pow...

Resolved! Question about charge pump of the L6395 driver

Hi everyone,I am using two mosfet as a switch (in order to open or close a contactor, turn-on or turn-off some PCBs, etc, not high frequencies are required), one high side mosfet and one low side mosfet. I want to control them with the L6395 driver.W...

SPV1050 - can LDO pins be grounded?

Hi, I am designing an application using the SPV1050. I am not using the LDO function, and am only using the SPV1050 for charging my battery.I have tied LDO1_EN and LDO2_EN to ground. Can I safely ground the LDO1 and LDO2 pins as well in this configur...

Getting real time ADC data out of STPM32

Apart from the V_RMS, I_RMS, power and energy (all aggregated), is it possible to output the ADC readings real time over SPI? I am looking to get 8k samples of I and V out of it. As of it was a pure ADC, with the filtering, but without the calculatio...

Fanuc30 by Associate III
  • 1146 Views
  • 0 replies
  • 0 kudos

Resolved! TL431 Marking Code (431CH)

Hi,Please help with the "TL431CDT"There is "H" symbol on the marking code (431CH)What does it mean?There is nothing is the datasheet (marking 431C without H).Best regards and thank youLuca

LMich.1 by Associate
  • 2215 Views
  • 2 replies
  • 0 kudos