Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hello team, I am now using STEVAL-STWINKT1 board to realize low-power online monitoring. But when I put the board into stop mode, the current consumption is still about ~10mA. Is that normal? And any solutions to reduce the power consumption? Thanks, Xiao

Hi, here are the steps I conducted:Disable all unused sensors; stop all timers; stop ADC. Enter stop mode: ( HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);Use LPTIM1 to wake up.And here are my questions:I used integrated current ...

YXiao.3 by Associate
  • 865 Views
  • 0 replies
  • 0 kudos

STEVAL-IPM30B

Hello.Can this module work in configuration as typical H bridge with controlling only 2 phases for brushed dc motor? Trigerring signals for third phase would be grounded.I see that recomended input voltage is from 125V - 400 V DC. Can this modul oper...

L5987A Regulator Noise and Voltage issues

Hello,I am using an L5987A voltage regulator to power a ublox LISA-U200 cellular module as specified in the LISA-U200 integration manual on page 23, figure 7. I have been having issues regarding high noise under load and completely incorrect voltages...

0693W000004IrJXQA0.png 0693W000004IrJNQA0.png 0693W000004IrJ8QAK.png 0693W000004IrIyQAK.png
LLawr.1 by Associate II
  • 986 Views
  • 1 replies
  • 0 kudos

STPMIC1 simulation models

Hello all,I'm designing a custom board based on MP1 familly and I'm using the STPMIC1APQR PMIC. To validate my design, I would like to simulate it. ​Is there any SPICE (Or IBIS etc) model of the PMIC available that can allow me to progress on that po...

Resolved! Quote for T1635T-8I

Looking out for a quote of about 5'000pcs. of T1635T-8I (Snubberless™ 16 A Triac).Who can help to find them easiest? Thanks for efforts

RMart.9 by Associate
  • 1123 Views
  • 1 replies
  • 0 kudos