Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
I have the board, I have downloaded all of the data and guides that I can find but there is no mention of AC IN voltage range. I would like to drive a small 400V induction motor. 400VACrms would mean 566V peak across the capacitor at no load.I note ...
Hello Madam/Sir,@Cristiana SCARAMEL We are developing a PMSM motor drive for an industrial application. This application is for Sugarcane Juice machine where we require to provide instant high torque for a shorter duration.I have developed a PMSM dr...
Hi,I am working with the stusb1702 device. I downloaded the datasheet but informations are missing. As software ingineer i am interested about the detail of register. Can I have a project example using the stusb1702 in sink role or full datasheet ?Si...
Do the integrated circuits L9823, E-L9823, E-L982301 differ or are they identical?Are they still in production?
Hi Everyone, this is my first post here.I am trying to drive a triac BT134 directly from the ATTiny816 processor. The goal is to drive the triac in Quadtrant 2 and 3. I have referred to the note by ST for negative power supply. Please see attached im...
At the datasheet at figure 7 you use CMC befor connecting it to DC2DC.I connect the PM8805 to DC2DC LTM8027.If I don't put the CMC will it be worng?BRShmuel
Using STM32F103C8T6 and Current transformers(A input) onboard current transformers