Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RHFL7913A, Power-Up

Hello, we are using the RHFL7913A to provide a negative supply for operational amplifiers. When we first supply the positive voltage to the op-amps, there is a positive voltage at the output of the RHFL7913A that is clamped to 0.4V by a protection di...

MKuebler by Associate
  • 970 Views
  • 0 replies
  • 0 kudos

High voltage conversion (1000V to 25V) for low power application - Are there some application circuit close to those values?

Hi, For a project I'm working on, I need to design a 3.3V power source (to power a microcontroller and measure circuit), the max load should be about 100mW. I only have a voltage source around 1000V next to it and I have to use it to make the 3.3V vo...

MLoua.1 by Associate
  • 1775 Views
  • 1 replies
  • 0 kudos

Resolved! Question about internal Vref of STPM32 chip

STPM32's document DS10272 states that Vref is 1.18V.However, if you install the "STPM3x Evaluation Software" program provided by ST and select the EVAL-STPM32 board in Configuration, Vref is set to 1.2V.which value is correct?In addition, if you look...

0693W00000aJYEEQA4.png 0693W00000aJY2xQAG.png 0693W00000aJYDVQA4.png 0693W00000aJYDpQAO.png
ckim.2390 by Associate II
  • 1790 Views
  • 2 replies
  • 0 kudos

Switch between VBAT and VDD without removing VDD

My device has various connected sensors and peripherals. The device is intended to go to sleep for extended periods of time before waking up and taking measurements. Currently, the main VDD is a large external battery and VBAT is a coin cell used to ...

MVeen.1 by Associate II
  • 2324 Views
  • 2 replies
  • 0 kudos

L6470 motor current vs MIN_SPEED

I use L6470 in my application at a certain running current. When I vary the speed the motor current remains more or less constant as expected. As soon as I change (actually increase) the MIN_SPEED value, the motor current changes (decreses). Anyone k...

Rajzol by Associate
  • 796 Views
  • 0 replies
  • 0 kudos

Strong current peaks at the end of some 6-step phases

My team has designed a circuit board based on EVSPIN32F0251S1 and controlled by the "STSW-SPIN32F0251" firmware, using the configuration "6step_conf_sl_cm_spdlp.h". The motor is moving fine, but during some measurements, we found strong current peaks...

0693W00000aJGL2QAO.png 0693W00000aJGL7QAO.png
SSant.5 by Associate
  • 802 Views
  • 1 replies
  • 0 kudos