cancel
Showing results for 
Search instead for 
Did you mean: 

Battery charger solution

STLearner
Associate III

Hi ST experts,

Would like to know if ST has any recommendation on battery charging solution?

The battery pack requirement is 7.4V 2300mAH which is 2-cells construction.

The intention is to change from standalone battery charger IC to a smart charger solution whereby it can help to prolong the battery lifespan for example having trickle charging and battery health (SOC) to keep the battery charge to max 80% (this can be done by configurable through software or hardware) and depth of discharge to 50% or 25%

Appreciate with any suggestions which can meets above-mentioned requirements.

Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Winfred LU
ST Employee

Sorry. There is no solution fitting the requirements.

Battery charger portfolio:

https://www.st.com/en/power-management/battery-chargers.html