Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

POWERSTEP01 external step input

When using the external step input of the Powerstep01, will the internal logic also use the advanced fast decay mode and switch between micro and fullsteps if a given speed limit is reached?Or does the step input only count microsteps and not using a...

pf8645 by Associate II
  • 1162 Views
  • 1 replies
  • 1 kudos

What is max speed of POWERSTEP01 in steps/sec?

In the STPSIN software, it seems that I am limited to 15609.741 Steps / sec?(See picture below)With a 0.9 degree motor (400 steps / revolution)this limits me to15609 steps/sec * 1 rev/400 steps * 60 sec/1 minute = 2341 RPMIs this the maximum speed o...

0693W000001pkQVQAY.png
CBeif.1 by Associate II
  • 2852 Views
  • 4 replies
  • 0 kudos

Mastergan technical questions

Hello all,1) what is the recoverytime of the internal bootstrap diode from the mastergan4L2) why this diode need a parallel one for the frequencies above 500 KHzThanks for answeringGentleRV

GentleRV by Associate
  • 679 Views
  • 0 replies
  • 0 kudos

IPS1025H/IPS2050h datasheet update.

Hello,i'm using some ips2050h-32 and ips1025h-32 from last year. Checking the datasheets, on the revision history they result been modified on july 2023, on table1, FLTx pins. Compared to the old version, seems that now it's been added the disclaimer...

lgenn1 by Associate
  • 1353 Views
  • 1 replies
  • 0 kudos

VN7050AJ SEL0/1 unused pin state

Hello all, in whole datasheet for VN7050AJ is not mention about default state of pins SEL0 and SEL1, but there is information that those pins can be left unconnected. Is there an internal pull-down resistor which selects current sense for CS output? ...

Eiffel by Senior
  • 673 Views
  • 0 replies
  • 0 kudos