User Activity

Hi, Please, I still trying all the ways to have Perl so far I know I should recompile it but using the toolchain I having errors out of the box.echo ${CONFIGURE_FLAGS}--target=arm-ostl-linux-gnueabi --host=arm-ostl-linux-gnueabi --build=x86_64-linux ...
Hi All,Please I`m working on a project that uses kvssink ( Aws Kinesis Gstreamer Plugin) that project uses log4cplus and openssl what uses Perl. During the cross compilation there are many perl modules missing from the SYSROOT what is the latest Deve...
Hi Please,I`m having problem to run an QT application: # error while loading shared libraries: libQt5QuickControls2.so.5: cannot open shared object file: No such file or directory.Please, how can I add it to image ? Thanks [ ]
Hi Guys,Please I facing problem to have a QT application fitting the DSI screen,it sounds like it is 400x240 and not 800x480. I`m probably missing something on QTor on the STM32MP157C-DK2.Can someone please help-me to correct the resolution and how t...
Hi All, Please , I`m pretty new here but so far using standard layer it works correctly hover when trying to use the QT / Distro openstlinux-eglfs layers meta-st I`m getting error related to make-mod-scripts.ERROR: Task (/local/STM32MP15-Ecosystem-v...