STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! On STM32 CubeMX : FreeRTOS and Timebase Source not selectable ?

Hello dear ST community,I try to test FreeRTOS on the STM32MP1 for the Cortex-M4 and I encounter a problem: I've got the following warning: "When FreeRTOS is used, it is strongly recommended to use a HAL timebase source other than the Systick" Ok, bu...

Resolved! Module.symvers of openstlinux-4.19

I am trying to add a kernel module for USB serial devices following: https://askubuntu.com/questions/168279/how-do-i-build-a-single-in-tree-kernel-moduleIn order to build just the module, not a completely new kernel , I would need the Module.symvers ...

MBeck by Associate
  • 2955 Views
  • 3 replies
  • 0 kudos

Resolved! What is the process for initializing the OpenEmbedded build environment st-example-image-qt?

Hi,I have followed link...https://wiki.st.com/stm32mpu/index.php/STM32MP1_Distribution_Package#Checking_the_prerequisites5.1 Initializing the OpenEmbedded build environmentPC $> DISTRO=openstlinux-eglfs MACHINE=stm32mp1 source layers/meta-qt5/script?...

stmdelta by Associate II
  • 8720 Views
  • 10 replies
  • 0 kudos

What could be the reason that the application does not start/not shows up on ubuntu 18.04 lts? After removing thirdparty.jar application starts but I am not able to generate the code.

System:Distributor ID: Ubuntu Description: Ubuntu 18.04.1 LTS Release: 18.04 Codename: bionicJava version:java version "1.8.0_201" Java(TM) SE Runtime Environment (build 1.8.0_201-b09) Java HotSpot(TM) 64-Bit Server VM (build 25.201-b09, mixed mode)C...

John Doe1 by Associate III
  • 1172 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.