User Activity

Hi all, I would like to know if someone is experiencing the same issue as me. I've got a custom STM32MP157CAC dev board and everything is working fine until I enable the HW crypto in the Linux Kernel and I want to mount a EXT4 FS. (EXT2 is ok but as ...
Hi, I try to compile Android on the STM32MP1 following the Wiki and I'm hitting a problem :hico@debian-ha:~/work/st/android$ hico@debian-ha:~/work/st/android$ repo init -u https://github.com/STMicroelectronics/android-manifest -b st-android-9.0.0-201...
Hi ST team !During the process of finding a way to put our custom boards in production, I tried to use the STM32Prog mode on Uboot. This failed because in SPL, spl_board_load_image() is empty and can't download via USB OTG the SSBL.I found another wa...
Hi, I wanted to flash the EVAL board with the latest Android version and I've got this error (see attached file)Any idea ?Thanks !Best regrads,Anthony Harivel
Hello everyone,   I'm curently working on a custom STM32MP1 board with a QSPI Nor flash. The NOR Flash seems to work perfectly in Uboot Basic after the modification we have done. The Data are MD5 checked and the SPL is at address 0x0 of the NOR Flash...
Kudos from