Resolved! CAD ressources for X-NUCLEO-NFC04A1
X-NUCLEO-NFC04A1 can i get complete hardware design document
X-NUCLEO-NFC04A1 can i get complete hardware design document
For NFC read write application I'm using this part number ST25R3916 can suggest me how to design antenna
Hi! I develop access system using NFC(14443-A) tags on Windows(.NET) platform + USB ST25R3911B-DISCO. I need simple API to read/write my data to the tag (like person name or ID, nothing secure). What API(and library) I have to use? I'm lost in all po...
Can anyone suggest ,pls, what should be the sequence of the registers configuration for ST25R3911 as a 14443-A reader , and the mechanism for sending and receiving APDU commands. Taking into account that there is no possibility to use the library...
Hi,I want to detect NFC tag. For that I have a P-NUCLEO-WB55 + X NUCLEO NFC06A1.I have downloaded the zip file (en.X-CUBE-NFC6_v1.1.0) from ST with examples but they are for boards that aren't mine.I tried to:Generate a code for wb55 with CubeMXAdd f...
Is it possible to get the Altium pcb and schematic files for the ST25R3916-disco or nucleo just like the ST25R3911B-disco?
Hi ST,We bought a ST25RU3993-HEPV last year to evaluate the RFID chip and wanted to control it using SPI (see that question, where you already helped us). The master SPI is a Cortex A15.We managed to set-up SPI communication and to implement spiTxRx(...
We are developing a IC card skipass Reader product for ski resort market. I checked TRF7961 from TI, but it can provide only 200mW output power. In the datasheet of ST25R3916, this IC can give up to 1.7W output power. I wonder these two are same inde...
Hi everyone,I'm facing some issues while trying to understand if (and eventually how) it's possible to use a different antenna using an X-NUCLEO-NFC03A1 evaluation board.I know I may just use the bare ST25R95 chip and then realize an impedance matchi...