ST25 NFC/RFID tags and readers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to deal with I2C Communication for the slave x-nucleo-nfc07a1 in which ST25DV64KC incorporated and is interfaced with STM32WB55RG?

Hi Sir/Madam, I am working with I2C in x-nucleo-nfc07a1 where ST25DV IC incorporated interfaced with Nucleo-WB55 board, what is the slave address(device address) for this?I am firmware engineer, I have I2C Scanning program wherePreviously, I work wit...

BT.2 by Associate II
  • 1383 Views
  • 2 replies
  • 0 kudos

Resolved! How to deal with I2C Communication for the slave x-nucleo-nfc07a1 in which ST25DV64KC incorporated and is interfaced with STM32WB55RG?

Hi sir, I am working with I2C in x-nucleo-nfc07a1 where ST25DV IC incorporated interfaced with Nucleo-WB55 board, what is the slave address(device address) for this?I am firmware engineer, I have I2C Scanning program wherePreviously, I work with Tem...

BT.2 by Associate II
  • 1400 Views
  • 5 replies
  • 0 kudos

Resolved! HAL_I2C_Mem_Read_DMA fails to read

Setup in use:P-NUCLEO-STM32WB development board.X-NUCLEO-NFC04A1 expansion board with software pack ( NFC 4.2.05) Added : DMA support for I2C , .ioc cubeMX image attached.The issue is that I cannot read the ST25DV ID via I2C DMA read. I simply do not...

0693W00000Y7AjGQAV.png
DS.4 by Senior II
  • 754 Views
  • 3 replies
  • 0 kudos

Resolved! Out of Band Pairing

Hi,I have a project where we use the STM32WB55 with the ST25R3911B as NFC module for OOB pairing.I couldn't find any example for OOB pairing flow.My start point is the p2p_server example and I can see there are:BleApplicationContext.BleApplicationCon...

~Amit~ by Associate III
  • 2272 Views
  • 14 replies
  • 0 kudos