Setup in use:P-NUCLEO-STM32WB development board.X-NUCLEO-NFC04A1 expansion board with software pack ( NFC 4.2.05) Added : DMA support for I2C , .ioc cubeMX image attached.The issue is that I cannot read the ST25DV ID via I2C DMA read. I simply do not...
Hi everybody,I have a custom STM32 board. I'd like to use ANT7-T-ST25DV64KC dev board to use NFC functionnalities. I have red that I can use X-CUBE-NFC7 to communicate with this board.In my cube MX, I have choose custom/NFCTAG7, I can configure IC2/...
I'm trying to install the X-CUBE-NFC5 package in the stm32cubeMX but I can only install the NFC4 and NFC7, someone knows how can I install the desired package, I wouls appreciate your help thanks.
CubeMX has a number of templates for discovery boards but there doesn't seem to be one available for the ST25R3916 Discovery
I originaly added the CubeMX NFC firmware module and made a few builds with that library.Then I removed the NFC component and now every time I generate the code the folders lib_nfc\Target and lib_nfc are added to project resulting in a few warning.I ...
Hello,I found firmware a package from ST web for ST25 application: STM32CubeExpansion_NFC4_V1.5.2.But it is for STM32L0, L4 and F4 series MCUs. I tried to add the package in the STM32CUBEMX for STM32G0 MCU but it doesn't work. Any suggestion to deal ...
Hi All,I'd like to use ST25DV NFC chipset on my STM32F103x project.I have found there was X-NUCLEO-NFC04A1 evaluation kit of ST25DV supporting CubeMX.I'd like to include the firmware package of NFC04A1 on my CubeMX project to use its API.How can I do...
Hello I would like to know if there exists a cube project to edit the demo enviroment of the ST25DV Discovery kit?