ST25 NFC/RFID tags and readers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How about STM32l4 power consumption

我有一个能源供应项目,并购买了X-NUCLEO-NFC07A1和NUCLEO-STM32L476RG。但是,我在EN中使用了EH代码。X-Cub-NFC7,现在我想根据此代码降低能耗。我应该如何编辑代码,使STM32L4具有最低的功耗并且只能完成LED闪烁测试?

Resolved! M24SR64 with stm32

Hi everybody,I'm working on a nucleo-L476. I'll like to write some data in NFC tag M24SR64 (I'm using a dev board ANT-7-M24SR).First, I developped functions to read into ndef memoru on ESP32 dev board. It works well (I can read my message with ST app...

0693W00000WHjJAQA1.png 0693W00000WHjJUQA1.png
fab04 by Associate II
  • 430 Views
  • 3 replies
  • 0 kudos

Resolved! about IRQ pin in X-NUCLEO-NFC06A1

Dear Sir,When I read the document of X-NUCLEO-NFC06A1, I found that the IRQ pin is not connected to CN5. I wonder the demo sample provided inST25NFC_Embedded_Lib_ST25R3916_1.4.0\Projects\STM32L476RG-Nucleo\Applications\X-NUCLEO-NFC06A1 do not use ...

DSai.1 by Associate III
  • 279 Views
  • 2 replies
  • 0 kudos

Resolved! Hard fault (usage fault, invalid state), using X-CUBE-NFC03 and FreeRTOS, with STM32L4. Seems dependent on code/data size. Any idea where I should investigate ?

Hello,I am trying to develop a FreeRTOS application which need to detect/read/write an NFC tag.I managed to make the NFC part work (based on ST's example code), but after changing my task stack size, a usage fault occurs (FORCED, INVSTATE).After a fe...

Slan by Associate II
  • 805 Views
  • 6 replies
  • 0 kudos