ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST25r100 Two single-eded antenna driving

Hello, is there any additional documentation that supports this system diagram? My project will have one antenna that will be an RFID tag whereas the other antenna will be reader. Can ST25r100 support this use case? I'd like to have the ability to wr...

itzel_0-1767816403749.png itzel_1-1767816492447.png
itzel by Associate
  • 76 Views
  • 1 replies
  • 0 kudos

Resolved! ST25R3911 Cannot Read FeliCa Cards

I am using a custom PCB based on ST25R3911B + STM32F072C8T6, and I am encountering an issue where FeliCa cards cannot be read.Initially, I used the X-CUBE-NFC5 software package downloaded from ST’s official website, along with the integrated RFAL lib...

Qinh by Associate II
  • 158 Views
  • 2 replies
  • 0 kudos

Resolved! Mifare classic 4k auth using X NUCLEO NFC10A1

Hello everyone,I am using the X-NUCLEO-NFC10A1 NFC reader with an NXP MCU.I am able to successfully detect a MIFARE Classic 4K card using this reader.However, when I try to authenticate a sector for read/write access, I encounter an issue.I am sendin...

Resolved! st25r3916b phase awake

Hi,I am using the st25r3916b chip with phase awaken, wake-up timer range of 800 msec and delta 3.Once it wakes up, I go to read the value in the register 0x3A (Phase measurement display register) in order to check which is the difference between of t...

SG3 by Associate III
  • 273 Views
  • 2 replies
  • 0 kudos

Resolved! How to switch to I2C mode on STEVAL 25R3916B board?

Hi I am evaluating NFC function on your STEVAL 25R3916B board, but I would like to see how it works with the I2C interface. Currently, the default configuration is SPI.I have downloaded STM32CubeIDE and STEVAL-25R3916B_V2.1.0 project code, but am not...

LeoWu by Associate III
  • 1774 Views
  • 21 replies
  • 2 kudos

Resolved! NFC WLC using ST25DV64KC

Dear  STMicroelectronics TeamI am currently developing a wearable board (WB) that integrates NFC communication and wireless charging features. For this design, I am considering using the ST25DV64KC as the NFC Dynamic Tag and the ST25R3916B as the NFC...

aromog by Associate
  • 272 Views
  • 1 replies
  • 0 kudos