Hi everyone ! After successfully launched ST25R3911 (in 14443-A smart card reader mode) without RFAL , using only analysis of dialog on ST25R3911B-DISCO there was a need to implement an 14443-A emulator based on ST25R3916. With the DISCO everything i...
Can anyone suggest ,pls, what should be the sequence of the registers configuration for ST25R3911 as a 14443-A reader , and the mechanism for sending and receiving APDU commands. Taking into account that there is no possibility to use the library...
HelloHelp me understand the interpretation of the APDU command response.Hardware : ST25R3911B-DISCO , Logic analyser , Visa NFC cardAction: send custom APDU and parse response The problem is : non-identical data (APDU answ.) received through the...
Thank you . Here is what I managed to make from the files you provided... From reset (C1) until the 3916 is recognized by external devices as a card, there are five stages separated by IRQ Stage_1:Start Dir_cmd (&HC1) Reg_Wrie (&H01,&H1C) Dir_cmd ...
PCD or PICC ? I would be interested in both modes with your permission .Could you share a bit about your non-friendship with RFAL .....? In particular, I study and work with the exchange protocol at the level like: for example data exchange for ante...