Resolved! VHBR and ISO 14443-A
The ST25R3911B datasheet indicates it supports VHBR. In the RFAL code, there is default configuration for NFC-B VHBR rates, but nothing for NFC-A (ISO 14443-A).Are VHBR rates supported for ISO 14443-A?
The ST25R3911B datasheet indicates it supports VHBR. In the RFAL code, there is default configuration for NFC-B VHBR rates, but nothing for NFC-A (ISO 14443-A).Are VHBR rates supported for ISO 14443-A?
Hi everyone,I'm using a MB1054B CR95HF RF transceiver demonstration board. Is ST25DV equivalent to this product? or MB1054B CR95HF Is there any similar product?
I am new to NFC. Currently, I have an ST25dv16k NFC. I wrote the EEPROM using the example Arduino code provided in GitHub. I am trying to enable the energy harvesting feature. How will I assign EN_MODE register to 0. Please help.
We are prototyping a ST95HF NFC in combination with an embedded Linux board.Since we can only find Linux demo code for the ST3916 on your website wetried to combine the ST25r95 rfa library found in STSW-ST25RFAL003_v2.6.0with the Linux demo code foun...
Hello,I am trying to find an example or application note that describes how to do OOB pairing using an NFC tag and the STM32WBx series. Has anyone out there successfully done this before, or can you point me to some good information for doing this?T...
I am trying to read temperature from SL900A tag. As base I am using in SDK provided. demo_gen2GenericCommand . Although tag is accessible and I am able to read the memory when I try to read the temperature from TAG I always get the failure response.D...
Actually, I download ST25PC-NFC program on web and installed in a new Windows 10 to my computer. Unfortunately, the program cannot run properly. The program front page would pop out to screen and closed the window immediately.
I'm trying to get a X-Nucleo-NFC06A1 shield to work with a Nucleo-L433RC-P devboard. As far as I understand, the requisite software package for that is the X-CUBE-NFC6.Unfortunately, I can't get it to install either by the package manager ("Help->Man...
Hi,I'm trying to set the GPO static register to 0xF1 to get corresponding interrupts.I am presenting the password first and then configuring GPO register at address 0000.Here is the program-NFCTAG_StatusTypeDef Set_GPO_reg(uint16_t flags) // Here fl...
Unable to access memory bank of the temperature sensor to get the temperature data.Hi,I am working on ST25RU3993-EVAL board for reading the temperature from RFM3200-AFR temperature sensor.I am finding very difficult in reading the temperature code fr...