Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Encoder interface

Posted on November 21, 2012 at 17:51Hi everybody!I have a problem when i reading data from ENCODER to stm32f103rc. My code is in the following:/*      */#include ''stm32f10x.h''#include <stdio.h>#include ''main.h''#include ''stm32f10x_it.h''#include...

tvv_it by Associate
  • 2192 Views
  • 1 replies
  • 0 kudos

L6470 step loss

Posted on October 03, 2012 at 17:36In a L6470 the microcontroller sends a Move command in 128-microstepping type; then, after a zero is read in the busy flag (so the movement has finished), the absolute position is read but the value read is smalles...

jgarcia by Associate
  • 1234 Views
  • 2 replies
  • 0 kudos

how to get complementary output at timer CH1 and CH1N ?

Posted on October 18, 2012 at 10:23[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/how%20to%20get%20complementary%20output%20at%20timer%20CH1%20and%20CH1N&FolderCT...

Noisy feedback from LSM303DLHC for motor control

Posted on November 02, 2012 at 17:05Didn't find a better location to post, so excuse the perhaps slightly off topic question. I am using a LSM303 (accelerometer/magnetometer) for detection of pitch/roll/attitude angles which then go through a PID co...

0690X00000605BTQAY.png

MOS instead of L6230 with stm32

Posted on October 26, 2012 at 13:20Hello, I work with stevalifn003v1. When I'm looking the output signal from the micro (on JP1,2,3,4,5,6) to the driver l6230, 3 are constant and 3 are PWM. This signals goes to logical gate on driver. If I want to w...

STM32_FOC_ACIM

Posted on April 11, 2012 at 13:27helllo, i'm new comer in here. i have project with SMT3210-MCKIT, and i used IAR EWARM 4.42 for compiler. but when i rebuild all program from strarter kit i got error like this :'' Error[e16]: Segment CODE (size: 0x6...

nanda by Associate II
  • 1981 Views
  • 4 replies
  • 0 kudos

Does anyone knows about those equations?

Posted on October 22, 2012 at 19:43Dear All,I am studding the application note AN2794 entitle “1KW dual stage DC-AC converter based on the STP160N75F3�. At page 11 the equation for the filter inductor is Lmin>=(N1/N2)*Vin-Vout*(TonMax/�?Ι)From...