Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L6470 Power ON and RESET

Posted on June 20, 2014 at 07:29HiI'm using L6470.It works to move step motor a bit,when the Powered on.The motor's coil  Voltage was high between  the RESET turn high and First SPI communication is started.(Almost 10ms?CPU's order)I don't want to m...

Step-Clock Mode

Posted on June 17, 2014 at 11:15Dear all,I actually using two l6470 boards (to control two stepper motors), connected in daisy chain configuration also with STM32F4DIS-EXT.I don't understand very well how to control these drivers in STEP-CLOCK mode....

in-rush current control

Posted on June 03, 2014 at 01:40I am working on a large system that is comprised of several different subsystems supplied with AC mains. In order to control inrush current to the system I want to build a controller that switches on AC duplex outlets...

Winding noise during hold

Posted on October 25, 2013 at 00:06Hello, With L6472 I hear audible (high pitch) noise from motor when holding. volume of noise increase with increase hold current. It does not matter if the motor is loaded or not.When I look at winding with scope o...

ppostig by Associate
  • 1151 Views
  • 2 replies
  • 0 kudos

Noise in a stepper motor with L6472

Posted on May 29, 2014 at 18:05Dear Enrico, I have the same problem of the other customer; I find this problem with two different family of sanyo denki's stepper motor (you can find the datasheet in the attachment): Type 103H7126-0140 and Type 103H7...

fab by Associate
  • 648 Views
  • 0 replies
  • 0 kudos

[L6470] Absolut Positioning

Posted on May 22, 2014 at 17:52Hello, I tried to poistioning my motor with the SPI command GoTo_DIR(DIR,ABS_POS). But then the motor turns a long time. So i run the command GetAbsPos, drive one step and run the command again. I wonder that one step ...

L6235 internal logic and temperature ratings

Posted on May 14, 2014 at 18:21I have 2 questions that I've posted to online support but haven't received a response. (1) I need clarification on the BRAKE input function - does it always short the 3 HS mosfets, independent of the ENA signal? I have...

krspahr by Associate
  • 764 Views
  • 1 replies
  • 0 kudos

L6482 Speed issue

Posted on April 11, 2014 at 14:47Hi,I'm tring to use a L6482 using only speed (Run) command because we have to use the motor in speed mode. Acc/Del are on our control. Chip Acc/Del are set to infinite (0xFFF) and MIN_SPEED/MAX_SPEED at 0,0x3FF. STEP...

c23 by Associate
  • 1035 Views
  • 3 replies
  • 0 kudos

L6480 high current absorbtion

Posted on May 22, 2014 at 11:42Our application:We have a Stainless steel disc diameter 30 cm, thickness 1mm, coupled with a chain to a stepper motor. The mechanical reduction is 1.5 (means that speed disc is slower than motor speed). Speed range of ...

baeridan by Associate
  • 831 Views
  • 0 replies
  • 0 kudos