cancel
Showing results for 
Search instead for 
Did you mean: 

VIPer53 with a wrong protection mode

niuminghui2008
Associate
Posted on July 30, 2013 at 09:56

I used VIPer53 in my product,I found that some of them entered into overheat (about 65℃) protection mode after running 70~180 mins at out power was 17W, and my design output power is 30W at Vin=220Vac. Change another VIPer53 the circuit can work very well.

We use viper53, about 4 years, there has been no problem.However, starting in April, chip has not work properly. We compared the difference between old and new chips.Find chip printing appear to change.the old chip( ''ST@    CHN'')has a space between ''ST''mark and ''CHN''.but the new chip don't have the space.

The VIPer53 with something wrong need more 4~5 Watts than the one without problem at the same output load. 
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0