Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FOC Hardware configuration.

Posted on November 12, 2017 at 10:25I've opened the P-NUCLEO-IHM001_SINGLEDRIVE project.In Control stage parameters.h I see#define PHASE_UH_GPIO_PORT            GPIOA                                                                            #define...

How to protect the 3.3V stm32 line ?

Posted on November 10, 2017 at 13:52Hello, I'm facing an issue regarding the 3.3V line on my board that embeds a stm32. The board also embeds a radio module (WISOL SFM10R1). My problem is that at one moment my radio module seems to be blown because ...

HVLED001A with output power of 100W and 150W

Posted on November 07, 2017 at 22:32Hi there,I would like to design a led driver to supply a load of 100W and 150W using the HVLED001A but the eDesignSuite is not calculating the right transformer. According to datasheet of HVLED001A is possible to ...

SPV1050 Res and Cap Equations Help

Posted on October 31, 2017 at 00:52Hi,Please see schema below.With this circuit the cells in series are creating ~ 0.82V in office lighting.LDO2 output is only 0.5v.  This does not seem right. :)Can anyone at ST help with correct selection of R1-6 s...

0690X00000608njQAA.png

Viper 16LD, Non Isolated Buck Regulation issue

Posted on October 26, 2017 at 09:18The output Voltage expected is 6V and output is constant for 110VAC input. But the output is turning ON/OFF for 220V input. Please let me know to resolve this issue. 

0690X00000608l5QAA.png 0690X00000608kpQAA.png 0690X00000608l4QAA.png

STEVAL-ISW001V1 Inverter Arc Welder

Posted on January 10, 2017 at 10:59Hello!Has anyone worked with the STEVAL-ISW001V1 demoboard or has designed an inverter welder based on the demoboard schematics? My design is working well in normal operation but I have some issues with the short-c...

Resolved! Which parts are pin compatible replacements for the VN7140AJTR?

Posted on October 16, 2017 at 21:17Hello,I need to find suitable alternatives to the VN7140AJTR that can swapped in with zero board changes.Is there a complete list of replacement parts available?It looks like the VN7040AJTR is a pin compatible repl...

2x L4981A

Posted on October 19, 2017 at 09:15HI,I have to build a 3KW PFC. The main points are:- 3KW- AC and DC operation- Analog Design, no SoftwarePreferd:- CCM- InterleaveIs there an expaple how to use 2x L4981A wit extrnal out of phase synchronisation and...