User Activity

Hi. I have problem with connect to NUCLEO-WL55JC nucleo via ST-Link Utility. I am unable to connect with any option (hot plug, connect under reset etc.) or hardware reset to STM32WL55 MCU on board (there is some demo soft which is unable to erase). ...
Posted on October 11, 2015 at 16:32Hi. I have one question about AN4076 ''Two or three shunt resistor based current sensing circuit design in 3-phase inverters''. On the page 6, 10 we can see signals on shunt resistor. How it is possible it's bipola...
Posted on August 02, 2015 at 09:56Hello. Program flashed with ST-LINK and Keil uVision 5.1 without any errors. The problem is program start only after several resets.  Anyone had similar problem? Thanks for any advice.