Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What is the problem in circuit design with A6986 .

Hi. I designed the power conversion circuit with A6986.​After soldering of this pcb, I powered 24V on power line.​And the VIN pin(#15) was damaged.​I have no idea what is the problem.​when I design the circuit, I consulted the manual, and eval. board...

0690X000008AKopQAG.png
Rsi by Associate II
  • 2884 Views
  • 4 replies
  • 0 kudos

I'm looking for ST eZ12042 IC datasheet

Hello, I have switching power supply with some IC from STMicroelectronics with ST eZ12042 marking on them but i can't identify them and find datasheet. I will be grateful for any help​Thanks in advance!

SKole.6 by Associate
  • 945 Views
  • 0 replies
  • 0 kudos

Why two mosfets and two diodes were chosen for Bridge rectifier instead of 4 diodes in 3KW grid-connected PV system, based on the STM32F103xx STM reference design AN3095.

Hi,i am desining an inverter using STM reference design AN3095.i happen to notice that the bridge rectifier section has been implemented using two fets and two diodes.Why is that so?What is the significance in such a method?Why din't they use four di...

Amal Babu by Associate III
  • 1593 Views
  • 1 replies
  • 0 kudos

Powerline Communication IC

Hi,We have built devices that run on batteries and serve a specific task. For the future we also want to offer a wired solution, for better user experience and more features, that would drain the batteries faster. Since the wired solution already re...

Questions about motor driver drv8835

[I used a translator.]Hi,I run the motor in "drv8835 Fast DK Mode".​The following waveform appears on the oscilloscope.When the pulse is low, about 6~7V is outputIs it working correctly?Is it normal not to fall to 0V?When operating in Slow DK (phase ...

0690X000008ABPgQAO.jpg