Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to calculate the right Capacitor for Qi charging coil?

Dear Forum,currently I'm implementing a design with the STWLC33 and in the datasheet is a reference design for a coil with L = 8 uH and a C = 3.9 nF. I calculated the resulting resonance frequency and got about f = 90 kHz (with Cser and Cpar). Shoul...

EZueh by Associate
  • 800 Views
  • 0 replies
  • 0 kudos

Overcurrent protection function of L6470h

Hi,I designed a board with ​L6470h and tested it. I am confused with the Overcurrent protection function. It is shown that the capability of L6470h is 7.0 A peak current (3.0 A r.m.s.), but the MAX overcurrent threshold can be set to 6A in register...

KFan by Associate
  • 799 Views
  • 1 replies
  • 0 kudos

STEVAL-IPFC01V1 capacitor bank problem

Dear all,we are evaluating STEVAL-IPFC01V1 board which is a PFC converter and we are experiences problems when we change capacitor bank to larger value. At default board is equipped with4x470uF, which we later changed to 4x1000uF plus 4x470uF. If we ...

STPM34 Minimum measurement time for U/I RMS values

Hi.I have a load switched by Triac, on which I perform a measurement with STPM34.I need to perform a very quick U/I RMS measurement (load is switched on/off)RMS computation is said to be performed on a 200ms window.But it seems I need to perform a ùe...

SC1 by Associate
  • 1158 Views
  • 1 replies
  • 1 kudos

Resolved! Diode Capacitance

I am looking at using the STTH112RL diode in a gate drive circuit. I was trying to find the capacitance of the diode but it is not in the data sheet. Can you please send me that information?NOTE: This question and answer originated from a customer su...