Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Isolated Low-Power Capacitively Coupled Supply

Hi Guys, I'm designing a low-power isolated supply (3.3V, Max ~50mA) and am keen to steer clear of transformers as EMI is critical to the design and I've had some noise issues with my previous transformer-based design. I have been looking at using a ...

Resolved! LDO U3 at STEVAL-USBPD27S

Hi together,the VCONN voltage at STEVAL-USBPD27S is generated with a LDO. https://www.st.com/content/st_com/en/products/evaluation-tools/solution-evaluation-tools/psu-and-converter-solution-eval-boards/steval-usbpd27s.html#overviewUSB power delivery ...

DRH by Associate III
  • 1554 Views
  • 1 replies
  • 0 kudos

GPIO vs SPI for LED1642GW

Well, as you can see in the datasheet and the application note for LED1642GW, It doesn't use pure SPI, since it doesn't use CS but it requires the Latch Enable (LE) signal.I'd actually like to write an application to manage multiple LED drivers but t...

JFern.5 by Associate II
  • 3370 Views
  • 7 replies
  • 0 kudos

L9916 OTP programming problem

Hi,I am use L9916 for alternator project. I want to do OTP programming. but I could not succeed. I found only one document for programming. There are some issues that are not fully explained in the document.Field monitor pin, understood as the pin ca...

0693W000006HGx2QAG.jpg
OKesk.1 by Associate
  • 776 Views
  • 0 replies
  • 0 kudos

Where may I get sources codes for STEVAL-DPSTPFC1 board?

Hi All !This is my first question here so please excuse me if I wrong.My trouble: I can't found sources code for STEVAL-DPSTPFC1 Totem-pole PFC board. https://my.st.com/content/my_st_com/en/products/evaluation-tools/solution-evaluation-tools/psu-and-...

AKamb.2 by Associate
  • 752 Views
  • 0 replies
  • 0 kudos

We have to design programmable power supply as per below spec 1. Vin: 230VAC, 50Hz 2. Vout: 0-120VDC or 20-120VDC, 12A max (variable with external control voltage from 0 to 5V) 3. Temp: -20 to +55 C Please suggest us any part number.

Hi,We have to design programmable power supply as per below spec 1. Vin: 230VAC, 50Hz 2. Vout: 0-120VDC or 20-120VDC, 12A max (variable with external control voltage from 0 to 5V) 3. Temp: -20 to +55 C Please suggest us any part number, this is for G...

SA.9 by Associate
  • 571 Views
  • 0 replies
  • 0 kudos

STEVAL-VP12201F

I don't know why ST don't include the transformer winding details into the STEVAL-VP12201F ??I even cannot find it on Wurth Elektronik site, these complications make it impossible for us to use it in our products.Is there any help from ST around here...

SShah.8 by Associate
  • 744 Views
  • 0 replies
  • 0 kudos

STEVAL-VP12201B

What is the possibility to feed the eSTEVAL-VP12201B from PFC with 385VDC?Do I still need to apply any filter at the DC input of the eSTEVAL-VP12201B when feeding it from PFC?In another word, I would like to feed it from a PFC with 385VDC without L1 ...

SShah.8 by Associate
  • 586 Views
  • 0 replies
  • 0 kudos