Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L6599AT gate drive pulses appear unexpectedly

We noticed that there are pulses at the gate drive outputs (pins 15 HVG, & 11 LVG) during the ramp-up of the control voltage (pin 12 VCC).This is what we saw: when VCC reaches about 11V, a sequence of pulses appear on both LVG and HVG. First LVG went...

0693W00000AMIWxQAP.jpg 0693W00000AMIXlQAP.bmp 0693W00000AMIXHQA5.bmp 0693W00000AMIXMQA5.bmp
FBaro.11 by Associate II
  • 2121 Views
  • 3 replies
  • 0 kudos

L6599AT Questions Q1: STBY pin does not stop pulses on gate drive outputs. Q2: Datasheet confusion for: (a) Soft-Start, (b) LINE.

Question 1:In our circuit Pin 5 STBY is pulled down to 0V to instantly stop pulses on gate drives. But sometimes when STBY=0V we still see pulses at the gate driver outputs LVG, HVG. The datasheet does not mention that gate pulses may still happen.I ...

0693W00000AME41QAH.jpg
FBaro.11 by Associate II
  • 2297 Views
  • 3 replies
  • 0 kudos

Request for help with a smart balancer development.

Dear All,I would like to ask for your help in the following topic. I've got a new task to develop a special balancer to lift up different weights (from 20 to 50kg) without the need of changing it's spring force. The weight of the products has to be m...

ZKóka.1 by Associate
  • 1353 Views
  • 2 replies
  • 0 kudos