Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L9958SBTR missing VDDIO pin

Hello STM Community,I am attempting to interface a L9958SBTR h-bridge module with a STM32F031K6 MCU. The h-bridge module claims to support 3.3v logic levels, however the VDDIO pin which determines the logic level of the SPI SO (serial data out) pin i...

Braedan by Associate
  • 1266 Views
  • 0 replies
  • 0 kudos

Resolved! Help finding a datasheet

Hey all,I'm trying to locate the datasheet of the following device:I think that it is a Zener, but I am not 100% sure.I've done the usual "Google" for the text, but I can't seem to find it.Thanks.

MicrosoftTeams-image (19).png

How about STEVAL-SMARTAG1?

I have a project about using NFC to collect sensor information without power supply, but the current EH output energy cannot be directly connected to the nucleo voltage pin of STM32L476RG, so can I refer to the design of STEVAL-SMARTAG1, adopt the de...

M48T58Y-70PC1 timekeeper packaging

Hello, I need to replace a ST timekeeper model number M48T58Y-70PC1They are on an extended back order.  They have another battery model number 511-M48T58Y-70MH1F available, however the packaging is different.  Are there adaptors available where I wou...

aguarin by Associate
  • 1572 Views
  • 1 replies
  • 0 kudos

PD3.1 adpater topology

Dear experts,I am looking for a solution for PD3.1 adpater. below are my questions.which topology is suitable for PD3.1 adapter, ACF or AHB Flyback? could you please explain why?why the power below 65W, the topology is usually use ACF rather than AHB...

powerguy by Associate
  • 711 Views
  • 0 replies
  • 0 kudos

How about SL-CNWLC05801V1?

At present, I have contacted the project about NFC power supply, but there has been no progress. The energy output through the EH pin of ST25DV has not successfully powered L4(MCU). Currently we know that SL-CNWLC05801V1 uses STM8, can its MCU be pow...

Suppress Inductive Energy when Triac Fired at any angle.

  The above waveform attached shows input sinewave which is stepped down using transformer and I am using voltage based zero cross detection for firing Triac. Above waveform shows TRIAC is fired at almost 10% of Positive and Negative Half cycle. I w...

Screenshot 2023-08-30 065500.jpg pradeepwagre_0-1693461526213.png pradeepwagre_1-1693461738177.png

iso808 continuous current calculation

hello  I have gone through the datasheet of ISO808. In the datasheet  ILim is 0.7A but for Channel Output Current (continuous) it is mentioned as internally limited. could you please give data for that or Is there any formula to calculate per channel...

sabari1_0-1693465632969.png
sabari1 by Associate III
  • 990 Views
  • 0 replies
  • 0 kudos

Resolved! Looking fro high speed LED driver

Hello,Not sure that the product I'm looking for exist. It should behave like LED driver but after looked through different LED I didn't find a product that meet my requirements:can drive 1 ... 15 LEDs connected in serieshave a possibility to change c...

Pavel_47 by Associate III
  • 2274 Views
  • 3 replies
  • 0 kudos