Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-ISV020V1 - total resistance

Hi @Peter BENSCH I hope all is well with you,As mentioned in a separate subject, I use my solar panel connected to the STEVAL-ISV020V1 to charge my LiPo battery. I wonder if you can help me figure out the total resistance of the STEVAL-ISV020V1 board...

rsmqu_0-1708937446848.png
rsmqu by Associate II
  • 1481 Views
  • 2 replies
  • 0 kudos

Resolved! STWBC86 GPIO registers

Hello, I'd like to use GPIO00 ... GPIO04 as outputs to select the used coil from a coil array for power transmitting.  I've seen the i2c addresses of the GPIO's configuration at 0x30 and followed. I'm wondering what address is foreseen to read or wri...

Self biasing in Viper06HN can damage it !

I have a problem with viper06HN in non isolated flyback converter , I think that happens due to self biasing (the chip get its power from drain voltage not the aux winding) , this happens at startup and after that the chip power from the Aux winding ...

STM32U585 VCAP capacitor voltage

Hi, I am using STM32U585 IC. I have a question on VCAP (L10) pin capacitor requirement. In recent datasheet it is mentioned rated voltage of the cap to use >10V. Why is it recommended to use10V rated cap for a maximum of 3V on pin. I have a concern o...

Sample code

Hii,How can we get the sample codes for STEVAL-ISA172V2 evaluation board?

Sk9999 by Associate
  • 916 Views
  • 0 replies
  • 0 kudos

The question about STDES-PFCBIDIR

Hi,I have a question about the reference design of STDES-PFCBIDIR.What is the function of relay  K4?It connect the Neutral and centro_bus.Thanks.

Eric7 by Associate
  • 656 Views
  • 0 replies
  • 0 kudos

L6230 - simple BLDC driving with BEMF detection

Hello, I want to use l6230 for BLDC motor driving. I'm trying to use it in typical application from the attached picture.In this application is commutation drives through binary signal from CPOUT - zero crossing.Is commutation drives through a binary...

0690X000008vu1hQAA.png