E-L9823013TR
Hello!I would like to clarify, can I use octal low-side driver E-L9823013TR in daisy chain SPI configuration?Regards, Val
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Hello!I would like to clarify, can I use octal low-side driver E-L9823013TR in daisy chain SPI configuration?Regards, Val
Hi, In my current design, I am using LDFM50DT-TR LDO for 5V output which acts as a source for RFID transceiver circuitry. LDFM50DT-TR is preceded by MEV3S0505SC (Digikey link) whose output goes to LDFM50DT-TR, please check the attached image for more...
Hello everybody, I am currently designing a configuration utilizing two drivers to heat a mat, which is a resistor load requiring 24V and 3.3A. This component is commuted at 100 Hz. For this setup, I've employed two different drivers: the first one b...
Hello,we are making qualification stress tests on our custom STM32MP157 board. One part of these tests consist to power the board with custom ramps that simulate the worst power scenarios (as glitches, slow ramp, brownout and blackout).We use the P/N...
Looking at the ST spice model for STN4NF20L i see only .SUBCKT STN4NF20L 1 2 3 There is no text note in the spice model file as to what the assumed pin ordering may be. The nodes in the model have no helpful names like DRAIN GATE SOURCE. Yes I can f...
Hi Motor Hardware Guru's,I am contemplating adding a mode that holds the low-side FETs ON when the motor drive is idle (sometimes for months) Is there a mode whereby GLSx / low side FET outputs can be set to high or high impedance state in standby o...
Hi, I am looking for some very flexible 3 core cable for my soldering iron. The stock one on the soldering is very rigged. Heat proof and all that good stuff, tangle free as well. Thank you
I am working on a project using L4986A. I was trying to get a bode plot of a boost PFC using L4986A model on simplis but I could not do a Periodic Operating Point (POP) analysis due to the IC containing non-linear blocks.I am wondering if there is a ...
The datasheet suggest its suitable for SMPS / lighting power supplies. Not clear if they can be used for the inductive load at the output of the hotswap controller.