Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STWBC86 stops working after a few days

Hi,I have a array of 2x5 STWBC86 on a aluminium plate to make a charging station for multiple devices. They are all connected to a common 5V source and decoupled by a small filter of Ferrite bead and MLCC.After testing them for a while i let them res...

S3rr4 by Associate II
  • 6443 Views
  • 13 replies
  • 0 kudos

STSPIN250 PWM current control

Hi, I am a bit confused about PWM motor driving. Is Vref the same value as Vavg of PWM? I tried to calculate the value of PWM current control but there have the result is not the same current value as I measured from a test, here are the parameters;R...

6ueiz by Associate
  • 703 Views
  • 0 replies
  • 0 kudos

STLINK-V3PWR power monitor.

Hi  I have been using the  NUCLEO-LPM01A board to measure current on my product, but I require to read up to 180ma . I have had a look at the STLINK-V3PWR unit, and can someone please let me know if I can simply use this wil the cube monitor power pr...

Average power dissipation of LDP01 series TVS diode

We require a TVS or zener diode for a clamping application with high average power dissipation. LDP01-56AY does suit our needs, but the maximum average power rating is not described in the datasheet. Our application has an ambient of around 60 degree...

SPV1040T Not Working as intended.

Hello, I'm trying to use the SPV1040T MPPT IC to boost up the 1.5V I'm getting from the Solar Panel to 3.8V. When I Power ON the MPPT IC its output just follows the Input and i don't see any chances of voltage getting boosted up. Is there anything wr...

Stalin by Associate III
  • 28625 Views
  • 17 replies
  • 1 kudos

Identification of blown items.

Hi Can anyone id this st device please...Its from a porsche cayenne bms module...vehicle been in a crash and this has blown.... I have id from the another identical item on the board...st-6-6bky z916... This ive found is coming back as thishttps://ww...

PORSCHE 3 (2).jpeg PORSCHE 3 (4).jpeg
BHP4EVER by Associate
  • 2127 Views
  • 5 replies
  • 3 kudos

STEVAL-L99615C demo load doesn't work

Hi,Now I work with the STEVAL-L99615C board and have some problem with it. I don't have an 5-cell board, so I connect charger and all needed saignals directly to the board. The board is configured to work in HS. GUI demo version 2.0.0.  Emb. version ...

photo_2024-04-09_15-31-20.jpg
MXliv.1 by Associate
  • 1283 Views
  • 1 replies
  • 0 kudos

two questions using L6599

hi, I'm developing 48v 1kw.Is it possible to set the rising time within 50 ms using l6599ad?The datasheet uses Rss and RFmin to control the initial soft start, but it does not decrease to 400 to 500 ms at all. If you need a circuit diagram, I'll send...

Jyu.6 by Associate
  • 1284 Views
  • 1 replies
  • 0 kudos

Resolved! VN920D-B5 chip

HelloSince the VN920D-B5 chip is not available, I am looking for a replacement. I am looking for another system with similar parameters.Please help me.

pietia by Associate II
  • 2413 Views
  • 4 replies
  • 0 kudos