STM32MP235A - Example software for Camera application
Hi Team,We are planning to use STM32MP235A for an IP PTZ camera application. Do we have an example code for the same? If yes, kindly share the links to relevant resources.Thanks,Preethi
Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.
Hi Team,We are planning to use STM32MP235A for an IP PTZ camera application. Do we have an example code for the same? If yes, kindly share the links to relevant resources.Thanks,Preethi
Hi everyone,I have the STM32MP257F-DK development kit and I'm interested in flashing or building Android OS for it. So far, I've found some resources and guides for the STM32MP257F-EV1, but nothing specifically for the DK variant.From what I understa...
... in order to make a "Hello World" and be able to use it for more applications? Based on the steps of the ST wiki on the stm32mp257f-dk through a VirtualBox to be able to use Linux and configure the A35, we realized that when performing the last ...
I am running OPTEE OS 4.0 from openstlinux distro 6.0. When i build package optee-examples (I also tried to build examples manually) and try to run it I get the following error; D/TC:? 1 tee_ta_init_pseudo_ta_session:303 Lookup pseudo TA 8aaaf200-245...
Hi I have a board based on a STM32MP135F. I can see that CLK signal of my sdcard (SDMMC1) very look like a 50 MHz sinusoidal instead of a clock. I have tested with and without my 22 Ohm resistor on this line and I am now looking into the device-tree/...
I created a layer using bitbake-layers create-layer --priority 7 ../layers/meta-st/meta-my-custo-layer and created mkdir recipes-graphics/wayland/weston-init/ and created folder called files and append file weston-init_%.bbappend and in files i add...
Hello everyone,i'm working on a custom SOC based on ST32MP135 and LAN8710 ethernet phy chip.When the HAL_ETH_Init() code runs and sends the module reset by setting the ETH_DMAMR_SWR bit, the loop exits with the HAL_ETH_ERROR_TIMEOUT.The current inter...
Running through the instructions to flash an eMMC chip via STM32CubeProgrammer. Board is custom based on STM32MP157F-DK2, boots great off a SD card (SDMMC1). I can communicate and load uboot via both USB and UART... uboot can get basic data off the e...
Using board based on stm32mp135f MPU, my goal is to configure a GPIO pin (let's say PD0, already freed from using with CAN) as a simple GPIO Output, active-high, with pull-up.I read following ST Wiki entires:- Overview of GPIO pins,- GPIOLib overview...
I'm currently working with an IMX219 camera sensor connected to the STM32MP257-EV1 board. The camera is successfully streaming, and the pipeline appears correctly configured through media-ctl. However, I’m unable to use the dcmipp-isp-ctrl tool at ru...