Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

vnh5019 arduino shield sw drivers

Posted on February 05, 2014 at 09:13hi, do st offer some software application example for this EVAL-VNH5019-P2 pololu arduino shield? i have two high current application where would fit. one to drive a high current stepper motor. the second for a du...

download for STSW_PCC009V2Fw

Posted on February 26, 2014 at 19:53I have tried to download STSW_PCC009V2FW five times. Each time I press the download button, the error message URL not found shows up. The file STSW-PCC009V2 can be downloaded, which includes the IBUUI rapid test ...

mcl198 by Associate
  • 700 Views
  • 1 replies
  • 0 kudos

3 phase ACIM without Sensor Hall And Encoder And tacho

Posted on February 07, 2014 at 18:47hi guys, i would be very grateful if you tell me some information about  ACIM Motor Control a 6 step PWM Signal interfacing with 3x 120° without Sensor Hall And Encoder And tacho For Speed Controller regards,

htc by Associate
  • 724 Views
  • 1 replies
  • 0 kudos

Can L6206 be used as 4 half H bridges?

Posted on January 26, 2014 at 17:12I want to use the L6206 to drive 4 solenoids (one end of the solenoid each solenoid will be grounded) of 2.5amps each. Can this be done without damaging the IC. ? Also each of the bridges two halfs will not be driv...

gada by Associate III
  • 598 Views
  • 1 replies
  • 0 kudos

No connection to STEVAL-PCC009V2

Posted on February 24, 2014 at 20:34Hi everybody,I'm trying to get the EVAL6470H working, but the problems are begining at the STEVAL-PCC009V2. I can't get any connection via the ''dSPIN Evaluation Tool'' to configure the L6470.I reflashed the firmw...

buck-boost AC-DC convertion

Posted on February 24, 2014 at 15:45Good morning, we are looking for an configuration for our application LED driver. We are taking a look among your AN, for L6562 designing in buck-boost config. In the AN3111, at pg8, there is a not clear equation ...

carlo by Associate
  • 1555 Views
  • 1 replies
  • 0 kudos

Stepper control with L298 and L297

Posted on January 08, 2014 at 23:07Hi to all, my name is Cosimo and I need help about stepper driver.From an old printer I've get a bipolar stepper and now I'm trying to drive it with L298 and L297 configuration. Whitout the stepper the output of L2...

cosimo by Associate
  • 1560 Views
  • 3 replies
  • 0 kudos

L6470 BEMF calculations

Posted on February 12, 2014 at 00:59Hi,Is there an online version of the BEMF compensation tool?  I have a couple of boards from Sprakfun that are based on the L6470 but I'm having issues getting the performance out of the stepper motors that I thou...

rob23 by Associate
  • 1195 Views
  • 2 replies
  • 1 kudos

L293 shorting output problem

Posted on January 23, 2014 at 10:12I use L293 as an buffer and level shifter from 5VDC to 24VDC on two of our boards and it works perfectly except for one thing: shorting any of the outputs to GND kills the chip! Could you suggest me a solution to t...

milos2 by Associate
  • 1085 Views
  • 2 replies
  • 0 kudos