Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

transistor ST32d/127 p5one can anybody help

Posted on July 09, 2018 at 17:00ithey are from a heat zink on a 24v dc to dc motor control unit made in 2002 by sevcon model mos90b there are 2rows of 6 on the neg 6 input and 6 ouput  hi i have found a matching number stp50ne10

Difference between two types T-series Triacs

Posted on July 13, 2018 at 09:59I ordered a Triac with type number T1635T-8T for temperature controlling on a hot glue application. This was not the same comparing to the fried one I already have on the application with type number T1635T-8I. The di...

Can the high voltage L9907 Driver Circuit be installed?

Posted on July 12, 2018 at 16:39I want to do a motor drive with the l9907. I have STP315N10F7 Mosfet. But there is a problem. The driver says that it supports up to 54V, but I want to use the MOSFET drain pin with 85V. How can I do that?#motor-contr...

L6699D No load condition

Posted on July 11, 2018 at 14:49Hi All,I have a 500W PS build around the L6699D and everything is working good.Now I found 1 little thing:If I run the unit in No Load the output is 24Vdc if I take the input voltage (AC) away the output drops a littl...

steval-esc001v1 not detected

Posted on July 06, 2018 at 11:51HiI try to connect to the board using STLink-v2 using IAR. But i get an error that device is not connected.Board is powered from a 12V source. PWM lines are unconnected.What could be the problem ?#steval-esc001v1

Qi firmware for the STWBC-WA (STEVAL-ISB038V1T)

Posted on January 25, 2018 at 11:21Hello,I'm looking for the Qi firmware to be used with the wireless transmitter STWBC-WA (evaluation board STEVAL-ISB038V1T).The firmware (http://www.st.com/content/st_com/en/products/embedded-software/evaluation-to...

Bou Chta by Associate
  • 1253 Views
  • 3 replies
  • 0 kudos