Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TSM1011 PSpice Simulation

HiI want to use TSM 1011 to design a battery charger . But I do not find the pspice model. Please help me how to modeling this IC(For example, I do not know how to implement the circuit current sensing part in the PSpice)or please send me the library...

0693W000007DaoBQAS.png
Spour.1 by Associate
  • 727 Views
  • 0 replies
  • 0 kudos

How to read DEVCFG0 Register of LED7708 Driver

According to the data sheet of the LED7708 it is not clear to me how to read the DEVCFG0 register. Since the bits OVFW, OTAF, OCAD, SCAD, contain status messages, I would like to be able to determine the cause of a fault. The firmware of the STEVAL I...

Rookie38 by Associate III
  • 549 Views
  • 1 replies
  • 0 kudos

STEVAL-POE005V1 Synchronous MOSFET's ratings.

Dear Sir/Madam,In STEVAL-POE005V1 EVM (12V/8A) i have measured Vds voltage across the secondary synchronous MOSFET, the measured Vds across Q5 (STL90N6F7 with respect to STEVAL-POE005V1 schematic) is ~61V @84W output (with sharp spikes) but the rate...

KV.1 by Associate
  • 1046 Views
  • 0 replies
  • 0 kudos

VN570 to220-7 need datasheet

Hello to all. This vn570 to220-7 is located in a car seat heating control module. Can some one give more info about this part, analog to it or some information? Part is damaged. No control of heating, visible damage to part.

NDoyn.1 by Associate II
  • 3656 Views
  • 4 replies
  • 1 kudos

Resolved! About BLDC motor solution

There are two ways of BLDC motor solution. The one of solutions is EVSPIN32F0601S3 and the other is EVSPIN32F0601S1. I want to drive BLDC motor with sensor less. Which solution is match the goal? The motor specification is 100V D.C. 1A 100W.

TGoto.1 by Associate II
  • 1055 Views
  • 1 replies
  • 0 kudos