Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103RCT6TR

Hi, I need a inform for given part number "STM32F103RCT6TR". Kindly tell me. which is the interrupt pin for given part number.

murali by Associate III
  • 764 Views
  • 1 replies
  • 0 kudos

Harmonic Distortion measurement

Hello,We are using STPM33 IC in our design. I want to measure Harmonic Distortion. Can any one suggest me how to measure Harmonic Distortion?Regards,Kadam

kadam by Associate II
  • 1235 Views
  • 1 replies
  • 0 kudos

Design of ZCD TRIAC circuit

I'm not sure if I've designed the circuit for PWM power control of the hot plate correctly. The PWM output is a 3.3V MCU. I assume the PWM period 200 ms. The hot plate is 1000W, 220V, 50Hz.

ZCD_220_KMOC3063_Triac.png
DRich.4 by Associate II
  • 962 Views
  • 0 replies
  • 0 kudos

VND9012AJTR/VND9016AJTR switch issue

Hi all, I would like to ask you about VND9012AJTR/VND9016AJTR.1) When INPUT1 goes high (+5V) through 1k resistor, OUTPUT1 goes to +12V, OUTPUT0 goes to +2V. The same situation is with INPUT0 (=>OUTPUT0 goes to +12V, OUTPUT1 goes to +2V)Why? I want to...

STGAP2SiCD connected issue

Hello ,I'm using the STGAP2SiCD gate driver IC to my application as a power conversion unit.I have some question about VDD pin and each logic input's voltage level.In my application, I connceted 3.3V to VDD and used MCU PWM output pin to INA(3.3V),an...

Resolved! Pls help me identify this component.

I'm looking for an alternative product to this diode.  I can't find any data sheets to the original product myself, so im hoping you can help me out.   

1000034903.jpg
Zahnelf by Associate
  • 1057 Views
  • 1 replies
  • 1 kudos

Resolved! Marking B4?

hi Peter, have looked a lot around but i couldn't found what stand for marking B4.could you please help me? thanks a lot, Michele 

_mik81 by Associate II
  • 2341 Views
  • 4 replies
  • 0 kudos

Resolved! L6599A bootstrap diode

Hi,What would be the consequence if there is a bootstrap diode used from pin 12 (Vcc) to pin 16 (boot), as used in the old days. I know that this should not be necessary because of the internal bootstrap circuit. So, can both "ways of working" used i...

dekkersj by Associate
  • 1078 Views
  • 1 replies
  • 0 kudos

Triac BTA40 RD91

Morning everyone, We are planning to control a 30Amps resistive charge using the BTA40 RD91 triac. I have seen that the connector of this faston has the appearance of a male faston connector with a 3.3mm diameter hole. Faston connections are not desi...

DaniES by Associate
  • 1715 Views
  • 3 replies
  • 0 kudos

(STC3115) Effect of battery discharge on OCV measurement

How much error will occur in the SOC calculation results if discharge occurs during the initial OCV measurement?Also, is the OCV measurement timing other than the initial stage of charging? At that time, are you looking at the battery current and mea...

ddddumi by Associate
  • 879 Views
  • 0 replies
  • 0 kudos