STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP1 - MAC address

Greetings,  I have a few STM32MP1 boards. One of which I have configures the OS on, and custom applications.I copied the SD card and put it in another one.  The MAC address is the same. I read an STM article about the MAC address and "fuse sense 0 57...

STM32MP157f-dk2 'drm-backend' has not been destroyed.

I built my image to test flutter gallery application from meta-flutter/workflows/stm32mp15. My local.conf file can be seen below:ACCEPT_EULA_stm32mp15-disco = "1" IMAGE_LINGUAS = "en-us" TOOLCHAIN_HOST_TASK:append = " nativesdk-flutter-sdk" CLANGSDK ...

Gencay by Associate III
  • 1453 Views
  • 1 replies
  • 0 kudos

spidev_test

Hi,I like to use spidev_test tool:https://wiki.st.com/stm32mpu/wiki/How_to_use_SPI_from_Linux_userland_with_spidev#Installation_on_your_targetI am following this guide for compiling the tool by developer package:https://wiki.st.com/stm32mpu/wiki/How_...

pjanco by Associate
  • 1480 Views
  • 0 replies
  • 0 kudos

Resolved! Fast Image flashing in the manufacturing line

Dear ST team, Hope you're doing well.We have developed a custom board based on STM32MP151 with emmc. Currently, we are using STM32MP151 for  flashing. The problem is each flash is taking around 15 minutes time and it will be a critical issue in our p...

Resolved! Build fails - Label not found &SRAM

error is logged as > Label or path sram not foundThe DTS file at the failing line reads   &sram{ dma_pool:dma_pool@0{ reg = <0x50000 0x10000>; pool; }; };  I'm assuming this is to specify where the SRA...

LAK17AT by Associate II
  • 2086 Views
  • 3 replies
  • 1 kudos

Resolved! stm32mp15x emmc reboot stuck-up

Hi,I have a problem with hanging up my board occasionally when an issue from the console reboot.I read about and the internet says this is a problem with the EMMC memory's power cycle.So I followed by a linkhttps://github.com/orangepi-xunlong/openwrt...

MWoło.2 by Senior III
  • 1322 Views
  • 2 replies
  • 0 kudos