User Activity

Hi,We are working on developing a custom board that necessitates the immediate activation of a buzzer with a predefined frequency as soon as the board is powered up. We are exploring the feasibility of utilizing the PWM driver in U-Boot to achieve th...
Hi,We are currently working on a project that involves utilizing the STM32MP13X MPU. Our device operates in both ACM and Mass Storage Mode, and we would like to inquire about the process of obtaining a custom name for the virtual serial COM port gene...
Hi,Are there any references for configuring the I2S supply voltages in device trees for STM32MP135-DK.From the I2S module currently we are getting the output level as 5V, is that expected or is there any way to change that from 5V to 3.3V.
Hi,Is it possible to utilize the PCM1754 DAC as a Sound card with the ALSA Framework on OpenSTLinux?According to the documentation, the PCM1754 functions as a Hardware-controlled DAC, eliminating the need for additional drivers. Therefore, is it nece...
Kudos given to