STM32 MPUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Power Consumption Data for STM32MP25 Series

Hi MP2 Champ ! Is there a table that summarizes the power consumption data of STM32MP25 series by use case?I can find data for MP1 series, but I can't find simple data for MP2 series except datasheet. Thanks.Best Regards, Jack

JackCha by Associate
  • 38 Views
  • 0 replies
  • 0 kudos

Resolved! Missing bootfs Partition in Yocto TSV Image Layout

Hi, I am trying to create an image for writing to NAND memory.The problem is that when generating a TSV file using Yocto, I get a layout without a bootfs partition.In this case, it is unclear how to load the Linux kernel and the DeviceTree.Can someon...

Piratkin by Associate II
  • 417 Views
  • 17 replies
  • 2 kudos

STM32MP255F - High Speed ADC Interface

Hello   I would like to interface the STM32MP255F to high-speed ADC like AD8285 or MAX1127 using these ADC's parallel interface. Is it possible to perform such interface while using the STM32MP255F GPIO lines?   Thanks.

sem_z by Associate
  • 173 Views
  • 1 replies
  • 0 kudos