STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Check error code for UART4

We made a new board with STM32MP157FAC1.I tried booting with SD card with STM32MP1 Starter Package image of STM32MP157x-EV1.I am inquiring about the following error. NOTICE: CPU: STM32MP157FAC Rev.ZNOTICE: Model: STMicroelectronics STM32MP157F eval d...

LeeJaewon by Associate III
  • 1038 Views
  • 1 replies
  • 0 kudos

STM32MP157 A7 and M4 communication

Hi,I'am also using  STM32MP157C-DK2  to communicate between the A7 and the M4 using the Virtual Uart (OPENAMP and IPCC).I was trying to use STM32MXCube to configure the peripherals but the STM32MP157C-DK2 board is not available instead CubeMX has STM...

mpeton by Associate II
  • 1435 Views
  • 3 replies
  • 0 kudos

MP135FAE baremetal with ThreadX

Hello everyone, i'm starting a baremetal project on a MP135 and i'm facing a issue when I tried to configure ThreadX.I've already saw the issue in another post :https://community.st.com/t5/stm32-mpus-embedded-software/creat-a-simple-bare-metal-azurer...

Manu31 by Associate
  • 794 Views
  • 1 replies
  • 0 kudos

Resolved! STM32MP1 A7 and M4 communication

Hi,I'm using STM32MP153C and I would like to communicate between the A7 and the M4 using the Virtual Uart (OPENAMP and IPCC).I'm using a custom distribution created using Yocto.When I initialize the virtual uart in the M4, /dev/ttyRPMSG0 is instantia...

ASega.1 by Associate III
  • 4230 Views
  • 6 replies
  • 2 kudos