Resolved! On the STM32MP157C-DK2, can I use/interface the available muRata 1Dx with M4 only (& not A7)?
On the STM32MP157C-DK2, can I use/interface the available muRata 1Dx with core-M4 only (& not core-A7)? I am not quite sure if the wifi module 1dx (U8 on the kit) is controlled by A7 or M4?Anyways, I want to interface it with M4. So, can it be possib...