STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! TouchGFX supported on STM32MP1?

Hi!   As the TouchGFX library is free for STM32, will it also support the STM32MP1 running under Linux?   Regards Friedl

Friedl by Associate III
  • 3432 Views
  • 15 replies
  • 1 kudos

ADC input protection on STM32MP157C

Hi,I'm interested if there is ADC input protection against voltage transients and overvoltage inside STM32MP157C or I should add external protection for used pins? If I had to add external components do you have some recommendations?Best regards,Nena...

NGajic by Associate III
  • 574 Views
  • 2 replies
  • 0 kudos

Resolved! How to properly compile linux kernel for stm32mp157c-dk2 ?

Hi,I want to compile linux kernel for stm32mp157c-dk2, i followed guide in README.HOW_TO.txt and when i run command "make ARCH=arm O="$PWD/../build" multi_v7_defconfig fragment*.config" in point 5. I get following errors:/opt/st/stm32mp1/stm32mp1-ope...

La1 by Associate III
  • 1227 Views
  • 4 replies
  • 0 kudos

Platform selection for new drone survey device

Hi, I am helping establish a reliable drone survey product, performing low-bandwidth sense operations and image detection for on-board analytics. This unit responds to what it reports, performing control & maintenance when needed.Unit:- Drone w/steer...

Justin1 by Senior
  • 408 Views
  • 0 replies
  • 0 kudos

Qt uses 'eglfs' to display performance problems

Qt uses 'eglfs' to display. After configuring this 'hwcursor', use Qt to display the card on HDMI. The touch screen will also get stuck. When the QT_QPA_GENERIC_PLUGINS environment variable is deleted and the mouse is plugged in, the mouse cannot be ...

0693W000005D1YAQA0.png 0693W000005D1YZQA0.png 0693W000005D1ZSQA0.png
User.44 by Associate II
  • 1882 Views
  • 2 replies
  • 0 kudos

Resolved! Changing the eMMC pins with OTP

Hello,I have a custom board based on STM32MP151-C with an eMMC on the following pins:SDMMC2_CK PE3 (AF09)SDMMC2_D0  PE6 (AF07)SDMMC2_CMD   PG6 (AF10)I read that the ROM expects the the SDMMC2_D0 pin on PB14 so I need to change it by using values from...

ANiko.3 by Associate II
  • 2928 Views
  • 10 replies
  • 0 kudos